Hi!
I tried to convert our current S32K148 project from RTD 1.0.0 to RTD 1.0.1
In the current project we are also using the FreeRtos and Lin/Lwip Stack.
But i it seems that there is not such support for those stacks at the moment.
Do I have to download some other software packages to get this functions (like at RTD 1.0.0)?
Or are those stacks not supported at the moment?
And if not can you give me an estimate when this packages will be available for the RTD 1.0.1?
Regards
Christof