For the Peripheral Clock of S32R274

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

For the Peripheral Clock of S32R274

1,090 次查看
578294688
Contributor II

I am new to S32,and I read the "HOWTO: Create a Blinking LED Project (MPC5748G) ",I have some questions:

1,For the I/O,is the Clock of the SIUL2 enable or disable?

Why have this question,   pastedImage_1.png

In this example,I find two functions of Clock,but I can't get some information from the functions.And I read the Reference Manual,I find that the peripheral's clock is supported by the PBRIDGE_n_CLK.

pastedImage_2.png

Enable the clock or Disable the clock?Need the function "CLOCK_SYS_Init()"?

Thank you!

标签 (1)
0 项奖励
2 回复数

825 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

To learn more about what settings could be used for the S32R274 MCU, please review the included examples for that part. We have many available and they are well documented. Please ensure you have installed the latest updates to have access to all of the available examples.https://community.nxp.com/docs/DOC-340769 

pastedImage_1.png

Hope it helps,

Mike

0 项奖励

825 次查看
578294688
Contributor II

OK!Thank for your help,I would read the demo code.

0 项奖励