For the Peripheral Clock of S32R274

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For the Peripheral Clock of S32R274

1,069 Views
578294688
Contributor II

I am new to S32,and I read the "HOWTO: Create a Blinking LED Project (MPC5748G) ",I have some questions:

1,For the I/O,is the Clock of the SIUL2 enable or disable?

Why have this question,   pastedImage_1.png

In this example,I find two functions of Clock,but I can't get some information from the functions.And I read the Reference Manual,I find that the peripheral's clock is supported by the PBRIDGE_n_CLK.

pastedImage_2.png

Enable the clock or Disable the clock?Need the function "CLOCK_SYS_Init()"?

Thank you!

Labels (1)
0 Kudos
2 Replies

804 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

To learn more about what settings could be used for the S32R274 MCU, please review the included examples for that part. We have many available and they are well documented. Please ensure you have installed the latest updates to have access to all of the available examples.https://community.nxp.com/docs/DOC-340769 

pastedImage_1.png

Hope it helps,

Mike

0 Kudos

804 Views
578294688
Contributor II

OK!Thank for your help,I would read the demo code.

0 Kudos