Flexram and Flexnvm cycle durability of the S32K1xx chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexram and Flexnvm cycle durability of the S32K1xx chip

Jump to solution
532 Views
ZEROOO
Contributor IV

Hello

    Please help solve a problem, the Flexram of S32K1xx chip is configured to simulate eeprom, and this analog eeprom refers to a space starting from 0x14000000, right? According to the manual AN12003, the cycle durability of simulated eeprom is about 100K. We have some differences on whether this 100K refers to flexram starting from 0x14000000 or flexnvm starting from 0x10000000, so please help to confirm it, thank you.

Labels (1)
0 Kudos
Reply
1 Solution
517 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @ZEROOO,

It is the endurance of the records in the EEE (FlexRAM (at 0x1400_0000)).

It depends on the number of records in EEE and the size of the EEE Backup flash (FlexNVM (at 0x1000_0000))

The endurance is 100k provided the ratio between EEE and EEE backup is 16.

danielmartynek_0-1704964601052.png

Please use the calculator:

danielmartynek_1-1704967085469.png

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

 

Regards,

Daniel

View solution in original post

3 Replies
518 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @ZEROOO,

It is the endurance of the records in the EEE (FlexRAM (at 0x1400_0000)).

It depends on the number of records in EEE and the size of the EEE Backup flash (FlexNVM (at 0x1000_0000))

The endurance is 100k provided the ratio between EEE and EEE backup is 16.

danielmartynek_0-1704964601052.png

Please use the calculator:

danielmartynek_1-1704967085469.png

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

 

Regards,

Daniel

516 Views
ZEROOO
Contributor IV

Hello,

    Flexram start address here is 0x14000000, FlexNvm address is 0x10000000, durability refers to Flexram, if flexram is not configured to simulate eeprom, is it the same cycle durability as ordinary ram?

ZEROOO_0-1704967496616.png

 

0 Kudos
Reply
501 Views
danielmartynek
NXP TechSupport
NXP TechSupport

I just fixed the addresses in my previous post.

Yes, the FlexNVM is not partitioned for EEE, the FlexRAM is just an SRAM and the FlexNVM is the DFlash.

DFlash endurance:

danielmartynek_0-1704969096076.png

 

Regards,

Daniel

0 Kudos
Reply