Failed to read memory @ address 0x00000000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to read memory @ address 0x00000000

Jump to solution
7,893 Views
longli
Contributor I

Hi,

When I try to run debug mode, the consoles reports the following errors. I use the sample codes(LPUART_s32k144) in SDK and my device is s32k144(64pins). while I found the sample codes is for s32k44 100pins.  The same codes I can flash or run debug on your provided EVB.

How can I set the 64pins in NXP IDE?

what should I do to solve the fowllowing error?

Starting target CPU...

Reading all registers

WARNING: Failed to read memory @ address 0x00000000

Removing breakpoint @ address 0x000004C0, Size = 2

WARNING: Could not remove breakpoint @ address 0x000004C0

ERROR: Failed to set breakpoint at 0x000004C0

WARNING: Failed to read memory @ address 0x00000000

Labels (1)
0 Kudos
Reply
1 Solution
2 Replies
6,940 Views
razva_tilimpea
NXP Employee
NXP Employee
3,994 Views
Lita
Contributor II
The ide I am using is S32DS.3.5 and no Components Library is found.how do i?
0 Kudos
Reply