Connect 6 cameras on Bluebox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connect 6 cameras on Bluebox

1,347件の閲覧回数
ying_gis90543
Contributor I

Hi,

I learned from this that NXP bluebox can connect 8 cameras. Then I click into the description of S32V2 Vision MPUs and it mentions the supported camera options is as below

1.jpg

I would like to connect 6 cameras in my project. May I have your suggestion which combinations I should buy ?

I ask this question because I see MAX9286S32V234 can only connect 4 cameras. Thank you in advance.

Sincerely,

Chianeng

タグ(2)
0 件の賞賛
返信
1 返信

1,287件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem  is
done only via tickets. This Community is not appropriate for questions
of this kind. If you wish to receive feedback from NXP Technical Support
with respect to this question, please:

  •     register on NXP Website with your corporate e-Mail address.
  •     open a Support Case.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信