Comparing power draw in 'STOP1/STOP2' mode vs VLPR/VLPS on S32K146

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Comparing power draw in 'STOP1/STOP2' mode vs VLPR/VLPS on S32K146

跳至解决方案
1,220 次查看
Farnam
Contributor II

I'm using the NXP Power Estimation Tool (PET).

For STOP1 and STOP2 power savings modes, the max power draw is listed as 8 mA and 9.2 mA respectively. It seems a bit unexpected that the power draw in VLPR and VLPS is listed as 1.57 mA and 37 µA, respectively.

I would think that the power estimation for the STOP modes should be less than that of VLPR and VLPS modes, especially given that STOP modes specify little to no peripherals to be active.
Can anyone shed some light on this for me?

标签 (1)
0 项奖励
回复
1 解答
1,205 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Farnam

you can take a look at the AN5425, the chapter 3.Power modes description

https://www.nxp.com/search?keyword=an5425&start=0

VLPS:Places the chip in a static state with Low Voltage Detect (LVD) operation off. This is the lowest-power mode in which pin interrupts are functional.

STOP:Places the chip in static state. LVD protection is maintained.

在原帖中查看解决方案

1 回复
1,206 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Farnam

you can take a look at the AN5425, the chapter 3.Power modes description

https://www.nxp.com/search?keyword=an5425&start=0

VLPS:Places the chip in a static state with Low Voltage Detect (LVD) operation off. This is the lowest-power mode in which pin interrupts are functional.

STOP:Places the chip in static state. LVD protection is maintained.