Can't use the Processor Expert for MPC5746R or MPC5743R

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't use the Processor Expert for MPC5746R or MPC5743R

跳至解决方案
1,957 次查看
rupingliu
Contributor I

Hi,

   We found that it can't use the Processor Expert tool when we “New” a project for MPC5746R / MPC5743R in S32 Design Studio for Power Architecture 2017.R1 .

   The S32DS had been updata to "S32 Design Studio for Power Architecture 2017.R1 Update 7 ", but it was still can't find the usable SDK.

   Can someone help us to figure out it?

   Thank you !

标签 (1)
0 项奖励
回复
1 解答
1,779 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

在原帖中查看解决方案

2 回复数
1,780 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

1,779 次查看
rupingliu
Contributor I

Thank you very much for your answer.

0 项奖励
回复