Can't use the Processor Expert for MPC5746R or MPC5743R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't use the Processor Expert for MPC5746R or MPC5743R

Jump to solution
1,878 Views
rupingliu
Contributor I

Hi,

   We found that it can't use the Processor Expert tool when we “New” a project for MPC5746R / MPC5743R in S32 Design Studio for Power Architecture 2017.R1 .

   The S32DS had been updata to "S32 Design Studio for Power Architecture 2017.R1 Update 7 ", but it was still can't find the usable SDK.

   Can someone help us to figure out it?

   Thank you !

Labels (1)
0 Kudos
Reply
1 Solution
1,700 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

View solution in original post

2 Replies
1,701 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

1,700 Views
rupingliu
Contributor I

Thank you very much for your answer.

0 Kudos
Reply