CMU on S32K118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMU on S32K118

2,862 Views
wei_w_he
Contributor IV

Dear Officer,

In S32K118, there are 2 CMU (clock monitor unit) can be configured to monitor FIRC. Does any SDK API support for it? (e.g. PE to configure and generate the code?)  And why there is no interrupt index defined for CMU in S32K118.h? Or it is covered by RCM_IRQn? 

Can we have a simple application code to demonstrate how to use these CMU?

Thanks and best regards

He Wei

 

Labels (1)
0 Kudos
Reply
4 Replies

2,796 Views
DavidMunoz
Contributor II

Hi everyone,

Could you please share with me the mentioned example? I interested on this module as well,

Regards,

0 Kudos
Reply

2,850 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi He Wei,

The interrupt IRQn is defined in the S32K118.h header file.

danielmartynek_0-1601897711356.png

The SDK does not support CMU configuration though.

I will sent you a simple non-SDK example.

 

Best regards,

Daniel

 

0 Kudos
Reply

2,650 Views
taiguo_han
Contributor I

I am also interested in the CMU , could you send me the example?

0 Kudos
Reply

2,837 Views
wei_w_he
Contributor IV

Dear Dinel,

Tks a lot.

BR

He Wei

 

0 Kudos
Reply