CAN interface Demo is needed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN interface Demo is needed

跳至解决方案
2,321 次查看
frank_feng
Contributor II

Recently , I am going to use M4 core existed in S32V234 platform to implement some applications , However ,I found no demos on CAN interface in S32DS For Vision, My specific platform is S32V234-EVB , I wonder if anyone could support me with this demo on CAN inetrface . any help would be needed , thank you . 

标签 (1)
1 解答
2,099 次查看
stanish
NXP Employee
NXP Employee

Hi,

Actually there is a FlexCAN example available. It's based on s32V234 SDK v0.8.1 (EAR) that is currently part of S32DS for S32 Platform only.

S32 Design Studio 2018.R1 for S32 Automotive ARM Platform (Windows/Linux) released! 

I'd recommend you to install this version + S32V2xx development package as described in the release announcement. It can coexist with S32DS for Vision (you can have multiple versions of S32DS installed on one machine)

Import S32V SDK example into the workspace by selecting menu File -> New -> S32DS Project from Example:

pastedImage_6.png

Note:

  The VSDK should be integrated into S32DS for S32 Platform at the beginning of Q2/2019

Hope it helps.

Stan

在原帖中查看解决方案

1 回复
2,100 次查看
stanish
NXP Employee
NXP Employee

Hi,

Actually there is a FlexCAN example available. It's based on s32V234 SDK v0.8.1 (EAR) that is currently part of S32DS for S32 Platform only.

S32 Design Studio 2018.R1 for S32 Automotive ARM Platform (Windows/Linux) released! 

I'd recommend you to install this version + S32V2xx development package as described in the release announcement. It can coexist with S32DS for Vision (you can have multiple versions of S32DS installed on one machine)

Import S32V SDK example into the workspace by selecting menu File -> New -> S32DS Project from Example:

pastedImage_6.png

Note:

  The VSDK should be integrated into S32DS for S32 Platform at the beginning of Q2/2019

Hope it helps.

Stan