Adding Data to Specific Memory Area

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Adding Data to Specific Memory Area

跳至解决方案
2,526 次查看
dsilva
Contributor III

Hello.

I need to add some values in a specific area of s32k144 memory. I'm using s32ds 2.2.

I added a new area definition to the linker as follows:

"m_appheader(RX) : ORIGIN = 0x00006800, LENGTH = 0x00000400"

In the main.c file I added the following line:

__atribute__ ((section(".appheader"))) const FLASH_APPHEADER_INFO APP_HEADER ={ ...DATA...};

The compilation runs without errors, the appheader appears in the map file, but when opening the hex or bin the data was not added. The entire appheader region is set to 0xFF.

Is there any configuration needed in the compilation so that this data is not removed?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,513 次查看
dsilva
Contributor III

I founded the problem.

I was just adding the appheader in the MEMORY field, the addition in the SECTION field was missing.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,514 次查看
dsilva
Contributor III

I founded the problem.

I was just adding the appheader in the MEMORY field, the addition in the SECTION field was missing.

0 项奖励
回复
2,519 次查看
Joey_van_Hummel
Contributor IV

I assume it has to do with your APP_HEADER being constant and thus the access to the .appheader region is being optimized away.

0 项奖励
回复
2,517 次查看
dsilva
Contributor III

Hello,

 

I removed the "const" and it didn't work.

 

I also added an ''IF" to that const and it didn't work too.

0 项奖励
回复