About the installation folder of S32K1_ISELED_BETA_2.9.2.exe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the installation folder of S32K1_ISELED_BETA_2.9.2.exe

ソリューションへジャンプ
2,516件の閲覧回数
r_kikuchi
Contributor I
This page (https://iseled.com/products.html)
Refer to the NXP Installation Guide (S32K SDK ISELED Driver installation guide BETA 2.9.2.pdf)
ISELED Software (S32K1_ISELED_BETA_2.9.2.exe) was obtained from NXP.
1. Please tell me where to specify the folder after executing S32K1_ISELED_BETA_2.9.2.exe.
2. Please tell me the work content of "Note: Please make sure you uninstall previous SDK so that this variable will be empty."
0 件の賞賛
返信
1 解決策
2,333件の閲覧回数
dragosrachitan
NXP Employee
NXP Employee

Hello,

The ISELED driver should be installed over the S32K1xx_SDK_BETA_2.9.2 release that you previously installed. As I can see from your folder tree, you should select the folder from S32DS\S32SDK_S32K1xx_BETA_2.9.2

Best regards,

Dragos

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,334件の閲覧回数
dragosrachitan
NXP Employee
NXP Employee

Hello,

The ISELED driver should be installed over the S32K1xx_SDK_BETA_2.9.2 release that you previously installed. As I can see from your folder tree, you should select the folder from S32DS\S32SDK_S32K1xx_BETA_2.9.2

Best regards,

Dragos

0 件の賞賛
返信
2,333件の閲覧回数
r_kikuchi
Contributor I
Thank you.

A1. I was able to install safely.
A2. After installation, "S32DK_PATH -> C:\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_BETA_2.9.2" is added to the system environment variable.
0 件の賞賛
返信