with problem in isp_ov10640_quad demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

with problem in isp_ov10640_quad demo

6,710件の閲覧回数
huangzhong
Contributor II

I have problem in the demo of isp_ov10640_quad, I use four ov10640 camera (with isp) in our system and I want to use isp_ov10640_quad demo, so what should I do to make it work? Look forward to your reply ,Thank you! 

ラベル(1)
0 件の賞賛
返信
14 返答(返信)

5,470件の閲覧回数
liyu1
Contributor III

我这边干掉了初始化ov10640的相关代码,修改了max9286和 max96705的初始化代码。发现在图像有翻滚,以及图像颜色不对的情况 。

0 件の賞賛
返信

5,470件の閲覧回数
huangzhong
Contributor II

The problem which color is not correct, may be cause by the below factor:

   1.please check the camera or max9286 register configure value.

   2.the lcd display format is UYVY, but your camera data may be YUYV, so you should get the image and chect it in computer, if your image is correct, then you should change the YUYV data to UYVY when in display.

0 件の賞賛
返信

5,470件の閲覧回数
yunlongyu
Contributor I

请问你们的camera(ov0640)是哪里获取的?是NXP提供的嘛?你们ov0640的配置通过什么配置的?

0 件の賞賛
返信

5,470件の閲覧回数
yong_qian
Contributor I

同问,camera是从哪里获取的,带的isp是ov490吗,还需要使用soc上的isp吗

0 件の賞賛
返信

5,470件の閲覧回数
liyu1
Contributor III

你好!请问能不能将MAXIM_OV10640_InitComplex 您那边设置的值发给我参考一下。不甚感激

0 件の賞賛
返信

5,470件の閲覧回数
yunlongyu
Contributor I

你好,请问你们用的ov10640的camera是哪里获取的?

0 件の賞賛
返信

5,470件の閲覧回数
liyu1
Contributor III

你好。。我们也在用s32v234  ov10640 带isp环视。请问这个问题你解决了吗。如果没有解决。。咱们可以一起解决。我QQ:542270618

0 件の賞賛
返信

5,470件の閲覧回数
huangzhong
Contributor II

已经解决了,使用了ov10635的demo来修改,将graph里面的引擎改成ov10640,重新编译替换sdk里面的graph,然后就工作正常了。

0 件の賞賛
返信

5,470件の閲覧回数
liujialu_2024
Contributor III

isp_ov10635_quad run failed:Failed to grab image number 0 

and got green-color area in lvds display

root@s32v234evb:~# ./isp_ov10635_quad.elf                                                                                                                      
**************************************************************                  
** Omnivision Ov10635 quad demo using Maxim Ser/Des HW setup                    
** Description:                                                                 
**  o Maxim 9286 deserializer board with 4xOmnivision Ov10635                   
**    cameras each with 9271 serializer (on MipiCsi_0) expected as              
**    image input.                                                              
**  o ISP converts YUV422 10bit piexel data provided by the sensor              
**    to YUV422 8bit pixels and stores single camera images into                
**    separate DDR buffers.                                                     
**  o Resulting YUV 1280x800 image are displayed live using DCU.                
**                                                                              
*********************************                                               
                                                                                
** Usage:                                                                       
**  o ./isp_ov10635_quad.elf <camera channel> [<csi port>]                      
**                                                                              
** Options:                                                                     
**  o camera channel   1-5. 5: switch each camera between 150 frames            
**  o                      [default: 5]                                         
**  o csi port         0|1 [default: use graph's setting]                       
**                                                                              
*********************************                                               
                                                                                
** Example:                                                                     
**  o Run camera #2, MAXIM pluged in CSI #1.                                    
**    ./isp_ov10635_quad.elf 2 1                                                
**  o Run all camera, use graph's setting for csi port.                         
**    ./isp_ov10635_quad.elf                                                    
**                                                                              
**************************************************************                  
                                                                                
[  122.839000] Probing I2c client @ 0x6a on I2C bus #0.                         
[  122.843866] Generic camera I2c driver added successfully.                    
[  122.849113] Probing I2c client @ 0x40 on I2C bus #0.                         
[  122.854240] Probing I2c client @ 0x30 on I2C bus #0.                         
------------------- Hello world -----------------                               
[  122.984534] Probing I2c client @ 0x41 on I2C bus #0.                         
[  122.990691] Probing I2c client @ 0x31 on I2C bus #0.                         
[  122.999142] Probing I2c client @ 0x42 on I2C bus #0.                         
[  123.004330] Probing I2c client @ 0x32 on I2C bus #0.                         
[  123.010929] Probing I2c client @ 0x43 on I2C bus #0.                         
[  123.016114] Probing I2c client @ 0x33 on I2C bus #0.                         
[  123.022686] Probing I2c client @ 0x44 on I2C bus #0.                         
[  123.027862] Probing I2c client @ 0x34 on I2C bus #0.                         
Press Ctrl+C to terminate the demo.                                             
Framebuffer mapped at 0x7fa16ef000.                                             
Failed to grab image number 0                                                   
Demo execution failed.

0 件の賞賛
返信

5,470件の閲覧回数
435761040
Contributor II

我和你使用了相同的demo ,你应该也是在调带ISPov10640 max9286 的四拖一的板子吧?我也正在调这部分,可以一起探讨 QQ:435761040

0 件の賞賛
返信

5,470件の閲覧回数
liyu1
Contributor III

你好。请问您这边修改了关于max9286 和96705的相关代码吗?

0 件の賞賛
返信

5,470件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

In this doc - https://community.nxp.com/docs/DOC-335010  is described how to create project for ISP graph demo. 

Jiri

0 件の賞賛
返信

5,470件の閲覧回数
yong_qian
Contributor I

请问你们有ov10640 camera提供吗,是否带isp,带的isp是ov490吗,如果带isp,还需要使用soc上的isp吗,谢谢

0 件の賞賛
返信

5,470件の閲覧回数
bigwater
Contributor I

请问,你是ov10640&ov490吗?有调试成功吗?能否分享一下

0 件の賞賛
返信