why i use S32DS V1.2  compiling the project,  s-record Size is too small?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why i use S32DS V1.2  compiling the project,  s-record Size is too small?

1,722 Views
yangliujie
Contributor II

i use S32DS V1.1 compiling the project, the s-record size is about 3~7Mbit,Now i use S32DS V1.2 compiling the some project, but the s-record size only about 600~700kbit, As if deficiency some data.微信图片_20180131122412.png

微信图片_20180131122530.png

微信图片_20180131122752.png

0 Kudos
Reply
6 Replies

1,292 Views
yangliujie
Contributor II

how can i setting the S32DS that can generate the full s-record files?

0 Kudos
Reply

1,292 Views
jiri_kral
NXP Employee
NXP Employee

Normally is .srec file generated with all linked objects. The issue with your project can be also caused by project migration. There is change in linker file between version 1.1 and 1.2. Did you migrate project correctly? 

Here is doc related to project migration: 

https://community.nxp.com/docs/DOC-335361 

Jiri

0 Kudos
Reply

1,292 Views
jiri_kral
NXP Employee
NXP Employee

Hello, 

it is probably because of some project settings. It looks like that in v1.1 is unused flash filled by 0x00, in v1.2 is not unused memory in the srec file present. Is your project working or not?

Jiri

0 Kudos
Reply

1,292 Views
yangliujie
Contributor II

by flash the s-record with the V1.2,the project can't work,but V1.1 can

0 Kudos
Reply

1,292 Views
jiri_kral
NXP Employee
NXP Employee

Can you please share both srec files?

0 Kudos
Reply

1,291 Views
yangliujie
Contributor II

share both the different s-record files

0 Kudos
Reply