why i use S32DS V1.2  compiling the project,  s-record Size is too small?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why i use S32DS V1.2  compiling the project,  s-record Size is too small?

1,556件の閲覧回数
yangliujie
Contributor II

i use S32DS V1.1 compiling the project, the s-record size is about 3~7Mbit,Now i use S32DS V1.2 compiling the some project, but the s-record size only about 600~700kbit, As if deficiency some data.微信图片_20180131122412.png

微信图片_20180131122530.png

微信图片_20180131122752.png

0 件の賞賛
返信
6 返答(返信)

1,126件の閲覧回数
yangliujie
Contributor II

how can i setting the S32DS that can generate the full s-record files?

0 件の賞賛
返信

1,126件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Normally is .srec file generated with all linked objects. The issue with your project can be also caused by project migration. There is change in linker file between version 1.1 and 1.2. Did you migrate project correctly? 

Here is doc related to project migration: 

https://community.nxp.com/docs/DOC-335361 

Jiri

0 件の賞賛
返信

1,126件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

it is probably because of some project settings. It looks like that in v1.1 is unused flash filled by 0x00, in v1.2 is not unused memory in the srec file present. Is your project working or not?

Jiri

0 件の賞賛
返信

1,126件の閲覧回数
yangliujie
Contributor II

by flash the s-record with the V1.2,the project can't work,but V1.1 can

0 件の賞賛
返信

1,126件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Can you please share both srec files?

0 件の賞賛
返信

1,125件の閲覧回数
yangliujie
Contributor II

share both the different s-record files

0 件の賞賛
返信