where is PE in S32DS of ubuntu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where is PE in S32DS of ubuntu?

3,447 次查看
ZHOUMO
Contributor II

My S32DS compilation project worked fine in a Windows environment, but for some reason I needed to switch the compilation environment from Windows to Linux. In Ubuntu 16.04 environment, S32DS does not have PE function, I migrated from Windows projects can not be directly used in Ubuntu environment, what can I do?

0 项奖励
回复
6 回复数

3,440 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately Processor Expert/SDK is not supported on Linux host machine, there is note in Relase notes. 

 

Jiri 

0 项奖励
回复

3,430 次查看
ZHOUMO
Contributor II

If I want to migrate my project from Windows to Ubuntu, how do I compile it?

0 项奖励
回复

3,403 次查看
jiri_kral
NXP Employee
NXP Employee

If the project is based on SDK - it is not possible, SDK is not available on Linux host OS. 

 

Jiri

0 项奖励
回复

3,370 次查看
ZHOUMO
Contributor II

If I port the code generated by PE and SDK on Linux, can I compile it using IDE? If not, can you compile it using cmake or makefile? Is there a routine for this?

标记 (1)
0 项奖励
回复

3,368 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

yes, it is possible use it this way (using generated code as a regular code). You may also find helpful this document: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-SDK-based-example-code-as-st... 

 

Jiri 

0 项奖励
回复

3,443 次查看
ZHOUMO
Contributor II

S32ds_pa_2.1_up14.zip installed, problem still

0 项奖励
回复