tooltip trouble of s32ds 3.6.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tooltip trouble of s32ds 3.6.3

530 Views
LewisThin
Contributor III

hello, experts.

i met a problem when i peripheral registers view in s32ds v3.6.3.  The view is docked on the right of the main view and the with is a little narrow. when the cursor is over a register name, the tooltip appears and just under the cursor, then view can not be scrolled. i have to move my cursor and then scroll again. i think the tooptip got the focus at that time. is there any solution?

LewisThin_0-1756891832138.png

 

best regards!

Tags (1)
0 Kudos
Reply
2 Replies

278 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for delay. You can simply make the view wider or drag and drop the Peripheral registers tab to better place - for example down next debug console. 

If there is some strange settings in debug perspective - reset the perspective. Window -> Perspective -> Reset Perspective. 

I tested it with S32DS v6.4 and tooltip works as expected: 

jiri_kral_0-1760637339311.png

 

0 Kudos
Reply

190 Views
LewisThin
Contributor III

hi  jiri_kral,

my issue is that when the tooltip appeared, the view can not be scrolled.

LewisThin_0-1761624005956.png

 

Tags (1)
0 Kudos
Reply