these is no SCB registers in peripheral registers view in s32ds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

these is no SCB registers in peripheral registers view in s32ds

3,232 Views
LewisThin
Contributor III

I updated RTD plugins and SDK of S32K3xx recently and then I found that the SCB group was missing.

further more, I can not downgrade the sdk and plugins in the case of which there is no the old ones in the "S32DS extensions and Updates page".

LewisThin_0-1706947199020.png

 

 

0 Kudos
Reply
6 Replies

3,164 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for delay. I tested it with S32DS v3.5 and S32K3XX RTD v3.0.0 and there is no issue: 

jiri_kral_0-1707906826057.png

 

Please make sure, that you have updated all packages to latest version:

jiri_kral_1-1707906958327.png

 

 

0 Kudos
Reply

2,922 Views
LewisThin
Contributor III
maybe sth is wrong, i changed the workspace and the issue was solved
0 Kudos
Reply

2,279 Views
YulongHe
NXP Employee
NXP Employee

Hi,

I meet the same issue and found these tickets. I found the root cause that maybe you missed the SVD configuration in the S32DS debugger setting, and this works for me. See below:

2,266 Views
LewisThin
Contributor III

Tnanks for your reply. It works on my device. But I have a new question about the svd file.  see below. Could you pls give me more information .

LewisThin_0-1741859707789.png

 

Tags (1)
0 Kudos
Reply

2,252 Views
YulongHe
NXP Employee
NXP Employee

Hi, I can find this file in this path. FYI.

0 Kudos
Reply

3,026 Views
Janeting123
Contributor I

Hello, I encountered the same problem. My S32 design studio version is 3.4. The S32 Design Studio Debugger Core cannot be found in the available extensions list. The Emb register list ends at MCM_CM7.

 

0 Kudos
Reply