target device (S32K146F1M0M11) disappeared from target list in debugger interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

target device (S32K146F1M0M11) disappeared from target list in debugger interface

1,460件の閲覧回数
louis_pelletier
Contributor I

Hello,

I tried to debug my project and an error came up that I've never encountered before.

(I am using S32DS ARM R1 version)

louis_pelletier_0-1610561886360.png

I found that when I want to select the device, the S32K146 is not in the list anymore and crashes the debugger interface.

louis_pelletier_1-1610561939476.png

 

I tried updating the software of the S32DS (SDK, S32K146 support, ...) but didn't change anything. Even when I create a project from example with a S32K146 project it shows me the error. I also tried a fresh install and the error remains.

**EDIT**

I tried installing the design studio v2.2 and I didn't update the S32K1xx development package (v2.2.0) and the S32 Design Studio Development package (v2.2.1) and it worked. I wonder where the S32k146 device is lost in theses updates.

Best regards,

Louis Pelletier

0 件の賞賛
返信
2 返答(返信)

1,406件の閲覧回数
louis_pelletier
Contributor I

Hi,

 

The problem I encountered was specifically following the update of the SDK. Even in a new workspace (for both S32DS R1 and S32DS v2.2). I re-installed S32DS v2.2 and did not update the SDKs and it works fine for now.

0 件の賞賛
返信

1,418件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Louis, 

 

it is possible, that your workspace is corrupted. You can try to create new workspace. 

0 件の賞賛
返信