stuck in "launching : Configuring GDB" while downloading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

stuck in "launching : Configuring GDB" while downloading

3,427 次查看
Byungmin_Hwang
NXP Employee
NXP Employee

Hello,

While trying to download a sample code into S32K144 w/ EVB, the progress is stopped as below.

pastedImage_1.png

The console shows only initializing at this point as below.

pastedImage_2.png

Anyone who know the way to figure this out?

BR,

Byungmin

标签 (1)
0 项奖励
回复
2 回复数

2,058 次查看
jlu
Contributor II

has this problem resolved? I'm having exactly the same problem for S32DS for ARM 2.2 on a board with S32K118. The S32DS, the board, the P&E debugger all have worked until it stops working

0 项奖励
回复

2,910 次查看
stanish
NXP Employee
NXP Employee

Hi Byungmin,

I'd recommend you to use the latest version of S32DS for arm if possible:

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! 

S32 Design Studio for ARM 2018.R1 - Update 1 available

 

It includes the updated version of P&E GDB server (v3.4.5).

In case you are connecting/debugging over OpenSDA please check if you have the latest firmware (v1.19).

If you don't have please update the firware:HOWTO: Update OpenSDA Firmware on EVB 

If you are using Windows 10 it is highly recommended to download and install the latest drivers by P&E:

pastedImage_2.png

If it doesn't help please let us know the version of your S32K144 chip populated on the board.

Hope it helps.

Stan

0 项奖励
回复