siul2_port configuration and functional Group setting in s32ds 3.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

siul2_port configuration and functional Group setting in s32ds 3.6

ソリューションへジャンプ
1,085件の閲覧回数
rlaxortn
Contributor IV

i wanna make each port container(adc, pwm, can, uart and so on)

but i got a error about functional Group. 

error is there are some duplicated 'NAME' in the PortContainer. 

화면 캡처 2025-04-15 111945.png화면 캡처 2025-04-15 111958.png화면 캡처 2025-04-15 112628.png

 

when i write a other PortContainer, portpin Mode, level value, slew Rate is not read. and i get errors.

화면 캡처 2025-04-15 112553.png화면 캡처 2025-04-15 112611.png

 

1. is it imppssible for making multi portcontainer?

2. if it is possible, how it make that?

3. can i get codument or description for setting functional group and adding functional group?

thanks for regards.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,010件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer to the introduction in  Interacting with Digital Inputs/Outputs on MR-CANHUBK344 
I have added the portpin id 1,2,3,4 in container 0.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,068件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did you add another PortContainer in Pins Tool?

PortContainer_1_VS_0 Pins Tool.pngPortContainer_0 PortContainer_1 Peripheral Tool.png

I'm not sure if this is what you need. If not please let me know.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,029件の閲覧回数
rlaxortn
Contributor IV

@Robin_Shen 

i have questions. 

 

1. what is mean portpin id//?

portpin id is 5 in your post. 

@Robin_Shen 

 

what is meaning portpin id is 5 in your pic?

does container 0 already has portpin id 1,2,3,4?

 

exactly i don't know portpin id's meaning.

is that just index?

 

2. if i have assign all of pin in one container, is it has a problem? 

why s32ds has a continer? for managing pins???

thanks for regards

0 件の賞賛
返信
1,011件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer to the introduction in  Interacting with Digital Inputs/Outputs on MR-CANHUBK344 
I have added the portpin id 1,2,3,4 in container 0.

0 件の賞賛
返信