sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdk

2,685 Views
Anjalipurushothaman
Contributor III

while creating a new s32ds application project, while selecting tool chain(NXP GCC 9.2 FOR Arm 32-bite bare metal) , following next button and selecting the cores and parameters SDK IS NOT SHOWING.

 

 

Whereas while selecting NXP GCC 10.2 for Arm , SDK options are available(platformSDK_s32k3_s32k358, s32k358_sdk) 

0 Kudos
Reply
4 Replies

2,615 Views
Anjalipurushothaman
Contributor III

Please find attached While debugging, port is not showing up in the window. Checked the com port the board is getting detected , but in the debug configuration tab it is not showing

0 Kudos
Reply

2,617 Views
Anjalipurushothaman
Contributor III

Thanks for your clarification. It will be helpful if you could share any sample example code to execute on S32K3X8EVB-Q289 Evaluation board.

Blinking LED with Autosar

0 Kudos
Reply

2,600 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

When you create a S32DS Project from the Example you should be able to find two blinking LED examples for S32K358 (Port_Example_S32K358 and Siul2_Port_Ip_Example_S32K358).

Regarding the debug configuration issue this is going to be answered in your other post (s32ds 3.5)

0 Kudos
Reply

2,655 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

The S32K3 Real-Time Drivers Version 3.0.0 was developed and tested only with GCC 10.2 This is the reason why you are not able to select this RTD version when you select GCC 9.2.

 

B.R.

VaneB

 

0 Kudos
Reply