s32ds ubuntu 18

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32ds ubuntu 18

1,592件の閲覧回数
mauriruizl81
Contributor I

 

Hello,

I have just follow the instruction to install s32ds in linux ubuntu 18, all steps, and special care in the java ones, but when I am executing the binary "S32DS.3.4_b201217_linux.x86_64.bin" I have got this error,

 

Preparing to install
Extracting the installation resources from the installer archive...
Configuring the installer for this system's environment...

Launching installer...

An internal LaunchAnywhere application error has occured and this application cannot proceed. (LAX)

Stack Trace:
java.lang.IllegalArgumentException: Malformed \uxxxx encoding.
at java.util.Properties.loadConvert(Properties.java:574)
at java.util.Properties.load0(Properties.java:391)
at java.util.Properties.load(Properties.java:317)
at com.zerog.common.java.util.PropertiesUtil.loadProperties(Unknown Source)
at com.zerog.lax.LAX.<init>(Unknown Source)
at com.zerog.lax.LAX.main(Unknown Source)

What could I do?

many thanks.

 

 

0 件の賞賛
返信
2 返答(返信)

1,527件の閲覧回数
mauriruizl81
Contributor I

Hello, yes, sorry I found out what was going on, I had a string  "\u" in the PS1 environment variable, remove that and it went Ok. many thanks

1,529件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you met all the requirements for Linux OS mentioned in Install Guide (installing 32 libraries and so on)?

 

Jiri

0 件の賞賛
返信