s32ds PA v2.1 error while importing a file from SVN server

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32ds PA v2.1 error while importing a file from SVN server

2,264件の閲覧回数
Furkan_26
Contributor II

Hello everyone, first of all I apologize for my bad English. I am new to S32DS and SVN applications. I think I have successfully installed the applications. but when I want to transfer files to S32DS application via SVN I get an error. error " checkout operation for ' filedirectory ' failed. svn: E200030: invalid expression ". is writing. The error files appear at the last stage of the import process. I can see ".c" files on TortoiseSVN, but folders appear empty on S32DS. I hope I was able to explain my problem. The reason why I think I did the installation correctly is that my friend did not have problems with the same procedures.

タグ(1)
0 件の賞賛
返信
0 返答(返信)