s32ds PA v2.1 error while importing a file from SVN server

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32ds PA v2.1 error while importing a file from SVN server

1,191 次查看
Furkan_26
Contributor II

Hello everyone, first of all I apologize for my bad English. I am new to S32DS and SVN applications. I think I have successfully installed the applications. but when I want to transfer files to S32DS application via SVN I get an error. error " checkout operation for ' filedirectory ' failed. svn: E200030: invalid expression ". is writing. The error files appear at the last stage of the import process. I can see ".c" files on TortoiseSVN, but folders appear empty on S32DS. I hope I was able to explain my problem. The reason why I think I did the installation correctly is that my friend did not have problems with the same procedures.

标记 (1)
0 项奖励
回复
0 回复数