s32M276 Missing, but can't find the s32m276 development package

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32M276 Missing, but can't find the s32m276 development package

1,710 次查看
cuongtran
Contributor II

cuongtran_0-1688848291879.png

I am trying to install the linstack on S32K ds 3.5 and got the above message, it seems that s32m276 development package is missing and I could not find it on the download site.

Can you tell me where to get it?

thanks.

0 项奖励
回复
3 回复数

1,599 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cuongtran , 

Please can you provide the installation details, workspace log, and installation log. 

1. Workspace log from the path
 C:\Users\Public\[workspace]\.metadata  (or wherever your relevant workspace is located).

 

2. Installation log from

C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs (or wherever your relevant installation folder is located).

 

3. Installation details from:

Help -> S32Ds Extension and Updates -> Installation details.

Mehul_Patel_NXP_0-1689022206085.png

Thank you. Kind regards. 

- Mehul Patel

 

0 项奖励
回复

1,590 次查看
cuongtran
Contributor II

Thanks for your help. Here is the installation details.

Package: S32 Design Studio Platform package; Version: 3.5.3; Build id: 202306291736
Package: S32K3 Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 P07; Version: 3.0.0; Build id: 202306300010
Package: S32K396.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: S32K3xx development package; Version: 3.5.0 RTM; Build id: 202304051438
Package: S32K396 development package; Version: 3.5.0 RTM; Build id: 202303300921
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202109281337
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: S32K3XX.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: GDB Client for Arm Embedded Processors 12.1 Build 1702; Version: 1702; Build id: 202306220849
Package: S32 RTD AUTOSAR 4.4 Version 4.0.0; Version: 4.0.0; Build id: 202210310146
Package: S32K3.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.6.7; Build id: 202306291725
Package: S32 Design Studio Platform Tools package; Version: 3.5.3; Build id: 202306291736
Package: S32K39X Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 P07; Version: 3.0.0; Build id: 202306300010
Package: S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 P07; Version: 3.0.0; Build id: 202306300010

0 项奖励
回复

1,560 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately latest version of LINStack depends on S32M276 Dev and RTD package. RTD for S32M276 is available, but Development package is only for offline use. Previous LINStack version depends only on S32K3 packages. Please contact your local FAE to enable for you Download the S32M276 Development package. 

0 项奖励
回复