s32 _3.4 demo compile error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32 _3.4 demo compile error

跳至解决方案
1,809 次查看
Lv_Jm
Contributor II
    • When I compile the demo project, the following error occurs.

      • How can I fix this error

    • QQ截图20230427105701.png

0 项奖励
回复
1 解答
1,743 次查看
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.

在原帖中查看解决方案

4 回复数
1,788 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lv_Jm 

did you click on Update Code icon in the configuration tool?

This is copied from the example description from user manual:

lukaszadrapa_0-1682573773593.png

 

The button can be found here:

lukaszadrapa_1-1682573858158.png

 

Regards

Lukas

0 项奖励
回复
1,782 次查看
Lv_Jm
Contributor II

I HAVE done that but it still have errors when compiling

0 项奖励
回复
1,746 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

This error doesn't appear to be the true source of the issue. The incremental build is complaining the object files are not found. Try performing a 'Clean Project' first, then a full build and share the errors that result.

mikedoidge_0-1682951355623.png

Best Regards,

Mike

0 项奖励
回复
1,744 次查看
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.