"S32DS for ARM IDE" Tool Qualification Materials

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"S32DS for ARM IDE" Tool Qualification Materials

Jump to solution
1,433 Views
sunghou-kim
Contributor III

Hello, NXP Team!

I'm using "S32DS for ARM" with IAR compiler addon.

I have to show some evidences to a safety-estimator that IDE using now is good enough for safety usage.

Are there any ISO- or IEC- kind of certifications I can get from NXP regarding S32DS IDE's tool qualification?

Thanks,

Sunghou.kim

 

 

0 Kudos
1 Solution
1,391 Views
mikedoidge
NXP Employee
NXP Employee

Hello @sunghou-kim,

We do not provide ISO, IEC, or any other safety certification for the S32DS IDE.

If you are using the S32 SDK, and would like safety documentation, it doesn't exist for the SDK either. The S32 SDK is not safety qualified. To contact support for the S32 SDK for more details, please post a question to: https://community.nxp.com/t5/S32-SDK/bd-p/s32sdk

For safety qualified software, the AUTOSAR 4.4 based Real-Time Drivers (RTD) are provided for some of the newest NXP Automotive devices. For more information on the RTD, please review the following article: https://www.nxp.com/company/blog/broadening-autosar-access-using-real-time-drivers-rtd-software:BL-B...

For safety documentation on the IAR compiler, we suggest you contact IAR.

Best Regards,

Mike

View solution in original post

2 Replies
1,392 Views
mikedoidge
NXP Employee
NXP Employee

Hello @sunghou-kim,

We do not provide ISO, IEC, or any other safety certification for the S32DS IDE.

If you are using the S32 SDK, and would like safety documentation, it doesn't exist for the SDK either. The S32 SDK is not safety qualified. To contact support for the S32 SDK for more details, please post a question to: https://community.nxp.com/t5/S32-SDK/bd-p/s32sdk

For safety qualified software, the AUTOSAR 4.4 based Real-Time Drivers (RTD) are provided for some of the newest NXP Automotive devices. For more information on the RTD, please review the following article: https://www.nxp.com/company/blog/broadening-autosar-access-using-real-time-drivers-rtd-software:BL-B...

For safety documentation on the IAR compiler, we suggest you contact IAR.

Best Regards,

Mike

1,373 Views
sunghou-kim
Contributor III

Many thanks appreciated!

I will contact IAR.

 

0 Kudos