"An Internal error has occurred" when update example project on .mex file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"An Internal error has occurred" when update example project on .mex file

跳至解决方案
1,320 次查看
MVR
Contributor V

Hello everyone,

I'm trying to update an example about SPI, using S32K344 and S32DS 3.4. The SDK version is 2.0.1.

This is the error that I'm facing:

MVR_0-1730211965441.png

In the past I was not facing this error, but it started suddenly... What should I do?

Thank you,

MVR

0 项奖励
回复
1 解答
1,293 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,294 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

0 项奖励
回复
1,310 次查看
MVR
Contributor V

I tried to reinstall the S32DS 3.4 and also the RTD S32K3XX 2.0.1 and still I'm facing the issue:

MVR_1-1730227660199.png

 

Basically I'm trying to remove the SpiPhyUnit_0 from the "Lpspi_Ip_HalfDuplexTransfer_S32K344" example...

0 项奖励
回复