processor expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

processor expert

跳至解决方案
1,994 次查看
indusivaraman
Contributor I

I read that processor expert is not supported on Linux or at least it may not work. can someone please tell me is there a workaround other than build the SW in Windows environment. what does the processor expert exactly do?

标签 (1)
0 项奖励
回复
1 解答
1,776 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,777 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

0 项奖励
回复