powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory

6,830 次查看
guoht
Contributor II

error:  powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory\

S32DS for powerPC v2.1

MPC5748G-LCEVB_QSP/MPC5748G-LCEVB_Code_Examples_08242016.zip/hello

标记 (3)
0 项奖励
回复
8 回复数

6,343 次查看
yerik
Contributor I

Hi, there, the problem is because of the updating of S32 DS, you can just re-select ewl_c9x.specs in project properties as following screenshot and the Sysroot will be updated to the correct one automatically. And then you can pass the compiling. Blog1-2.png

Blog1-3.png

0 项奖励
回复

6,343 次查看
michaelbinz
Contributor III

I had the same problem, but cannot recreate my project, since it was not created from an example.

The cause of the problem is that the e200 tools were moved for S32DS 2.1.  The solution is to open the .cproject file of the project and replace all occurrences of 'S32DS/e200_ewl2' by 'S32DS/build_tools/e200_ewl2'.

jiri.kral@nxp.com‌:  Is there a way to accomplish the same without manually modifying the project file? People do not work only with examples, but are in need to migrate existing projects.

0 项奖励
回复

6,343 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

do you have installed these packages in your S32DS? (Main menu bar -> Help -> S32DS Extensions and Updates: 

pastedImage_1.png

0 项奖励
回复

6,343 次查看
wanbenzhou
Contributor II

Hello!

I have installed the above package.

My new project can be compiled.

But when I open the example project downloaded from the official website, it is not compiled, there will be the above error.

Who knows, give pointers.

0 项奖励
回复

6,343 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

Can you please share your project? 

Jiri 

0 项奖励
回复

6,342 次查看
wanbenzhou
Contributor II

Hello!

I use the existing routines on the NXP network, which leads directly to the compilation of the project.

All examples are in the attachment and you can try a project.

0 项奖励
回复

6,342 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this example set is for S32 Design Studio for PowerPC v1.1.  You can find similar examples in current S32DS release:

On main menu bar -> File -> New -> S32DS Project from Example:

pastedImage_2.png

 

pastedImage_1.png

Hope it helps. 

Jiri 

0 项奖励
回复

6,342 次查看
wanbenzhou
Contributor II

Does anyone know that this is a problem? The example of the official website download is compiled into the project.

0 项奖励
回复