error: powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory\
S32DS for powerPC v2.1
MPC5748G-LCEVB_QSP/MPC5748G-LCEVB_Code_Examples_08242016.zip/hello
Hi, there, the problem is because of the updating of S32 DS, you can just re-select ewl_c9x.specs in project properties as following screenshot and the Sysroot will be updated to the correct one automatically. And then you can pass the compiling.
I had the same problem, but cannot recreate my project, since it was not created from an example.
The cause of the problem is that the e200 tools were moved for S32DS 2.1. The solution is to open the .cproject file of the project and replace all occurrences of 'S32DS/e200_ewl2' by 'S32DS/build_tools/e200_ewl2'.
jiri.kral@nxp.com: Is there a way to accomplish the same without manually modifying the project file? People do not work only with examples, but are in need to migrate existing projects.
Hello!
I have installed the above package.
My new project can be compiled.
But when I open the example project downloaded from the official website, it is not compiled, there will be the above error.
Who knows, give pointers.
Hi,
this example set is for S32 Design Studio for PowerPC v1.1. You can find similar examples in current S32DS release:
On main menu bar -> File -> New -> S32DS Project from Example:
Hope it helps.
Jiri