new sds application project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

new sds application project

1,099 Views
Anjalipurushothaman
Contributor III

which library : new lib/lib nano

I/O Support : no I/O, Debugger console, real time print f

 

which options has to be selected while creating new application project, what are the differance

0 Kudos
Reply
1 Reply

1,074 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

This setting enables the semi-hosting support and configures input/output to print information to the console during debugging.

  • No I/O - no printing will be done.
  • Debugger Console - the output will be printed out to the console provided by the debugger specified in the Debugger setting.
  • Real-time printf with ITM - the Instrumentation Trace Macrocell (ITM) block provides a mechanism for sending data from your target to the debugger via the SWO trade stream.

 

B.R.

Vane.

0 Kudos
Reply