license of S32DS missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

license of S32DS missing

1,664 Views
GAODU
Contributor I

Hi:

My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me? 

S32-DS-VISION_V2018.R1_187191607

Activation code: C6C4-D203-BE38-84B1

Thanks.

0 Kudos
Reply
5 Replies

1,638 Views
GAODU
Contributor I

use  open   workspace   :

 

 

  • It's urgent. Please help me

  • I  can not use,please help me ,thanks.
0 Kudos
Reply

1,627 Views
GAODU
Contributor I

Uninstall and reinstall the S32DS software.An error message is generated when the following activation code is used.Please check it again.

 

S32 Design Studio for ARM v2018

Total Number of Licenses:100

Activation CodeFD88-476A-D03B-A42C

GAODU_0-1662538650715.png

 

 

0 Kudos
Reply

1,642 Views
GAODU
Contributor I

GAODU_0-1662517958324.png

I  can not use,please help me ,thanks.

0 Kudos
Reply

1,591 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

It's likely that you are having some issue with a firewall blocking access to the server. Perhaps try again but use the offline activation method. If this method fails, you may need to use another internet-connected device which can access web pages and is connected to a public wifi where there is no firewall and then use the offline activation method.

HOWTO: Activate S32 Design Studio - NXP Community

Best Regards,

Mike

0 Kudos
Reply

1,646 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

The entitlement for this activation code is set to expire in the year 2027. In fact, it was only just issued on 05 September 2022. What error message are you receiving?

Best Regards,

Mike

0 Kudos
Reply