Hi,
I am using the IDE 'S32DS for ARM 2.0', and I installed the 'S32K14x 0.8.6 EAR' S32SDK.
Now I want to update S32SDK RTM 3.0.2, so I download and install the 'S32SDK_S32K1xx_RTM_3.0.2.exe' file,
but I can't find '3.0.2' option in the 'SDK Management' window.
1. Should I add new SDK option manually?
2. When I use the Processor Expert tool, are the generated drivers of RTM 3.0.2 newer than EAR 0.8.6?
Regards,
Snaku