Hello
I am trying to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G to S32 Design studio using USB 2.0 cable for flashing only but I can not see any port added to my PC
the question is
how to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G to S32 design for flashing/debugging ?
is using an external debugger is necessary in all cases ?
Thanks
已解决! 转到解答。
Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first.
Jiri
Hello,
EVB MPC574XG-MB doesn't contain integrated debugger (like Open SDA) and you have to use external one - for example PE Micro .
I'm not sure if you bought mother board (MPC574XG-MB) together with daughter board (MPC574XG-324DS). For debugging you need both boards.
Jiri
Hello,
Thanks a lot for your answer. Yes I bought it with daughter board (MPC574XG-176DS) .
What about only flashing the MCU ? I do not need to debug for now Can I do that without external debugger ?
Thanks
Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first.
Jiri