how to connect MPC574xB/C/G EVB to S32 design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to connect MPC574xB/C/G EVB to S32 design studio

跳至解决方案
2,989 次查看
shadymohamed
Contributor II

Hello

I am trying to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G to S32 Design studio using USB 2.0 cable for flashing only but I can not see any port added to my PC

the question is

how to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G  to S32 design for flashing/debugging ?

is using an external debugger is necessary in all cases ?

Thanks

标记 (3)
0 项奖励
回复
1 解答
2,882 次查看
jiri_kral
NXP Employee
NXP Employee

Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first. 

Jiri 

在原帖中查看解决方案

4 回复数
2,882 次查看
jiri_kral
NXP Employee
NXP Employee

Hello, 

EVB MPC574XG-MB doesn't contain integrated debugger (like Open SDA) and you have to use external one - for example PE Micro . 

I'm not sure if you bought mother board (MPC574XG-MB) together with daughter board (MPC574XG-324DS). For debugging you need both boards. 

Jiri

0 项奖励
回复
2,882 次查看
shadymohamed
Contributor II

Hello,

Thanks a lot for your answer. Yes I bought it with daughter board (MPC574XG-176DS) .

What about only flashing the MCU ? I do not need to debug for now Can I do that without external debugger ?

Thanks

0 项奖励
回复
2,883 次查看
jiri_kral
NXP Employee
NXP Employee

Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first. 

Jiri 

2,882 次查看
shadymohamed
Contributor II

Thanks Jiri for your help

0 项奖励
回复