how to connect MPC574xB/C/G EVB to S32 design studio

cancel
Showing results for 
Search instead for 
Did you mean: 

how to connect MPC574xB/C/G EVB to S32 design studio

Jump to solution
231 Views
shadymohamed
Contributor II

Hello

I am trying to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G to S32 Design studio using USB 2.0 cable for flashing only but I can not see any port added to my PC

the question is

how to connect the EVB MPC574XG-MB: Evaluation System for MPC574xB/C/G  to S32 design for flashing/debugging ?

is using an external debugger is necessary in all cases ?

Thanks

Tags (3)
0 Kudos
1 Solution
124 Views
jiri_kral
NXP Employee
NXP Employee

Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first. 

Jiri 

View solution in original post

4 Replies
124 Views
jiri_kral
NXP Employee
NXP Employee

Hello, 

EVB MPC574XG-MB doesn't contain integrated debugger (like Open SDA) and you have to use external one - for example PE Micro . 

I'm not sure if you bought mother board (MPC574XG-MB) together with daughter board (MPC574XG-324DS). For debugging you need both boards. 

Jiri

0 Kudos
124 Views
shadymohamed
Contributor II

Hello,

Thanks a lot for your answer. Yes I bought it with daughter board (MPC574XG-176DS) .

What about only flashing the MCU ? I do not need to debug for now Can I do that without external debugger ?

Thanks

0 Kudos
125 Views
jiri_kral
NXP Employee
NXP Employee

Well - for flashing MCU you need some external debugger. It can't be done via USB. Anyway - if you connect USB - B (the the big squared one) port to your PC machine - you should see new COM port. This USB to COM converter can be used with MCU - but for this functionality you need to flash program into MCU by external debugger first. 

Jiri 

View solution in original post

124 Views
shadymohamed
Contributor II

Thanks Jiri for your help

0 Kudos