e_cmpwi issue: operand out of range (powerpc-eabivle-4_9)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

e_cmpwi issue: operand out of range (powerpc-eabivle-4_9)

2,759 Views
mschroeder
Contributor I

I am porting some existing (and probably long time working) code for SPC5645C (e200z0, e200z4) from Diab Compiler to S32DS_Power_Win32_v2017.R1_b171019

In the startup code I am struggling with the e_cmpwi instruction:

c-source:

MOVE_SYMBOL_ADDRESS_TO_REGISTER(__ROM_COPY_SIZE, r9);

/* Check length of SRAM data in ROM */
ASM2ID(e_cmpwi r9, 0);
/* Exit cfg_ROMCPY if size is zero */
ASM1ID(beq _ram_copy_end);

which becomes

366 ???? 7120E000          e_lis 9,__ROM_COPY_SIZE@ha
367 ???? 1D290000          e_add16i 9,9,__ROM_COPY_SIZE@l
368 ???? 1820A800          e_cmpwi 9,0
****  Error: operand out of range (9 is not between 0 and 3)
****  Error: missing operand
369 ???? 4182002C          beq _ram_copy_end

In EREF_RM the register value occupies 5 bits of the opcode and I could not find any constraint for register rA to be in the range 0...3. Also there is no "missing operand", so I feel quite confident that this is a bug.

Martin

Labels (1)
0 Kudos
Reply
5 Replies

2,208 Views
alexanderfedoto
NXP Employee
NXP Employee

Thats really not a bug.

You are using e_cmpwi mnemonic which is actually just an alias. There is no such instruction in PowerISA document.

Meaning of this alias was recently changed in binutils mainline.

See also compiler release notes chapter 3.2:

Opcodes and syntax for e_cmpwi and e_cmplwi aliases were changed. Use e_cmpl16i instead of e_cmplwi, and e_cmp16i instead of e_cmpwi.

0 Kudos
Reply

2,208 Views
mschroeder
Contributor I

Hi Stan,

I had already -Wa,-mregnames turned on and switched to Alex's suggestion which compiled fine:

__asm("e_cmp16i r9,0");
277 0262 70099800            e_cmp16i r9,0‍‍‍‍

By the way, is there a common way to access all the SPRs by symbolic name other than:

.set l1csr1, 1011
mtspr l1csr1, r5

Martin

0 Kudos
Reply

2,208 Views
alexanderfedoto
NXP Employee
NXP Employee

You can try always to use spr name as suffix of mt* or mf* instructions  like:

mfl1csr1 r1

mtl1csr1 r1

0 Kudos
Reply

2,208 Views
stanish
NXP Employee
NXP Employee

Hello Martin,

Thanks for the report! This is indeed a GCC VLE compiler bug.

I reported this into our defect tracking database under CMPE200GCC-182.

I'd recommend you to use direct instruction opcode as a workaround.

asm(".long 0x70099800");
70 09 98 00 e_cmp16i r9,0
‍‍

Regards,

Stan

0 Kudos
Reply

2,208 Views
mschroeder
Contributor I

Hello Stan,

many thanks four your super fast solution!

Best regards,

Martin

0 Kudos
Reply