dear all,
When I download the program to MPC5775E through PE, the following error is generated:
"error during flash programming. Terminating debug session."
with the console information as follows:
"Once Status Register Result = $0209
REM Set up MMU for Periph A Modules
REM Base address = $C3E0_0000
REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access
Once Status Register Result = $0209
REM Initialize all of the Main SRAM - 512KB
Initializing RAM from $40000000 to $4007FFFF.
Reset script (D:\Program Files\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\s32e200_mpc5777c.mac) completed.
MPC5777C Device detected.
PE-ERROR: Error downloading to the device.
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "59345" from 7224
Target Disconnected."
Can you tell me how this happened and how to resolve it.
tank you!
XiufengWang
Hi,
Are you using a custom board or an NXP evaluation board?
I'd recommend you to create a new dummy single core project for MPC57775E.
Build the project and debug via PE.
First I'd start with Debug_RAM build configuration - no flash programming involved.
Then I'd repeat the test with Debug_FLASH build configuration
If you are able to debug both - the issue is related to your custom project . Typically could be an issue in linker file (e.g. section placement into unavailable memory) causing programming algorithm to fail.
Hope it helps.
Stan
Thank you for your reply
I created an empty project, and I can download the program with Debug_Ram successfully, but the result is still the same error with Debug_Flash.
The board we use is a custom board
Hi,
could you check the reset signal while programming flash? Do you use SBC chip on your custom board?
Also I'd recommend you to instal the latest S32DS update (it includes the latest version of pemicro plugin):
Stan