can't read register values in mpc5748g

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can't read register values in mpc5748g

Jump to solution
3,834 Views
rahulramakrishn
Contributor III

Hi

I am trying to use the Ethernet in the MPC5748G LCEVB. I currently using the inbuilt code provided in the S32DS. While debugging the code PE Micro shows a warning: "PE-ERROR: Warning. Can't read registers while part is running".

Then a popup will appear that shows unable to detect the hardware. I think this is because the register is not readable. 

Please help me to fix this problem. 

Why PE Micro multilink universal can't read register values of MPC5748g while I able to execute the flex CAN program using the same configuration?

I attaching the console data of Ethernet program. Please find it.

Regards

Rahul Ramakrishnan 

0 Kudos
Reply
1 Solution
3,119 Views
jiri_kral
NXP Employee
NXP Employee

Hi Rahul, 

I played a bit with PE Micro timing settings - and for me is working this configuration:

pastedImage_1.png

It looks like that it is board depend. With some boards are default values okay, for some others not.

Jiri 

View solution in original post

0 Kudos
Reply
7 Replies
3,119 Views
jiri_kral
NXP Employee
NXP Employee

Hi, which example are you using? The SDK one - Enet PING or non-SDK enet_rmii_udp? If the non-SDK - please make sure that you are using launch group in debug session. This is multicore project and the Z4_0 is boot core.  

Jiri

0 Kudos
Reply
3,119 Views
rahulramakrishn
Contributor III

Hi Jiri

Do you find out the reason for this behavior? If you found it, Please share with me. I still having the same problem and I stuck here. I am waiting for your reply.

Regards

Rahul Ramakrishnan

0 Kudos
Reply
3,120 Views
jiri_kral
NXP Employee
NXP Employee

Hi Rahul, 

I played a bit with PE Micro timing settings - and for me is working this configuration:

pastedImage_1.png

It looks like that it is board depend. With some boards are default values okay, for some others not.

Jiri 

0 Kudos
Reply
3,119 Views
rahulramakrishn
Contributor III

Hi Jiri

Thank you very much for your support. Now my code is running without any error. Thank you very much.

Regards

Rahul ramakrishnan

0 Kudos
Reply
3,119 Views
rahulramakrishn
Contributor III

Hi

I am using enet_rmii_udp_z4_1 example. Launch group is used in debug

session. But I can't able to debug it. It shows that device is in reset

escalation mode. When power cycle the board it show that can't detect

device.

While examining the console I found a warning "PE micro can't read

register values". I have no idea why this happens. Can you help me to solve

this problem?

I am using MPC5748G LCEVB with S32DS and PE Micro multilink universal.

Thanks in advance

Regards

Rahul Ramakrishnan

On May 14, 2018 6:37 PM, "jiri.kral@nxp.com" <admin@community.nxp.com>

0 Kudos
Reply
3,119 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

good news - I can reproduce the issue on one of my boards (motherboard with daughter card) - but right now I don't know what is root cause. There is warning info about reset escalation, then board may be secured warning - and at the end I got the very same console output. I'll continue with investigation and let you know. 

Jiri 

0 Kudos
Reply
3,119 Views
rahulramakrishn
Contributor III

Hi

Thank you very much for your effort. I hope you can find a solution to the problem.

Regards

Rahul 

0 Kudos
Reply