Hi
I am trying to use the Ethernet in the MPC5748G LCEVB. I currently using the inbuilt code provided in the S32DS. While debugging the code PE Micro shows a warning: "PE-ERROR: Warning. Can't read registers while part is running".
Then a popup will appear that shows unable to detect the hardware. I think this is because the register is not readable.
Please help me to fix this problem.
Why PE Micro multilink universal can't read register values of MPC5748g while I able to execute the flex CAN program using the same configuration?
I attaching the console data of Ethernet program. Please find it.
Regards
Rahul Ramakrishnan
解決済! 解決策の投稿を見る。
Hi Rahul,
I played a bit with PE Micro timing settings - and for me is working this configuration:
It looks like that it is board depend. With some boards are default values okay, for some others not.
Jiri
Hi, which example are you using? The SDK one - Enet PING or non-SDK enet_rmii_udp? If the non-SDK - please make sure that you are using launch group in debug session. This is multicore project and the Z4_0 is boot core.
Jiri
Hi Jiri
Do you find out the reason for this behavior? If you found it, Please share with me. I still having the same problem and I stuck here. I am waiting for your reply.
Regards
Rahul Ramakrishnan
Hi Rahul,
I played a bit with PE Micro timing settings - and for me is working this configuration:
It looks like that it is board depend. With some boards are default values okay, for some others not.
Jiri
Hi Jiri
Thank you very much for your support. Now my code is running without any error. Thank you very much.
Regards
Rahul ramakrishnan
Hi
I am using enet_rmii_udp_z4_1 example. Launch group is used in debug
session. But I can't able to debug it. It shows that device is in reset
escalation mode. When power cycle the board it show that can't detect
device.
While examining the console I found a warning "PE micro can't read
register values". I have no idea why this happens. Can you help me to solve
this problem?
I am using MPC5748G LCEVB with S32DS and PE Micro multilink universal.
Thanks in advance
Regards
Rahul Ramakrishnan
On May 14, 2018 6:37 PM, "jiri.kral@nxp.com" <admin@community.nxp.com>
Hi,
good news - I can reproduce the issue on one of my boards (motherboard with daughter card) - but right now I don't know what is root cause. There is warning info about reset escalation, then board may be secured warning - and at the end I got the very same console output. I'll continue with investigation and let you know.
Jiri
Hi
Thank you very much for your effort. I hope you can find a solution to the problem.
Regards
Rahul