build project error as the following message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

build project error as the following message

1,338件の閲覧回数
hicensezhang
Contributor I

hicensezhang_0-1647508424547.png

when I build the project, the result report error as the image , could you help it? thank you

 

0 件の賞賛
返信
1 返信

1,030件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @hicensezhang.

What is the version of the S32K144 SDK you are using? S32 SDK RTM 4.0.3 is the latest.

I see that the make command in your screen capture shows as: make -j4 all

However, when I build this same project, the make command is: make -j20 all

Did you change some settings on this project?

Best Regards,

Mike

0 件の賞賛
返信