build project error as the following message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

build project error as the following message

1,343 Views
hicensezhang
Contributor I

hicensezhang_0-1647508424547.png

when I build the project, the result report error as the image , could you help it? thank you

 

0 Kudos
Reply
1 Reply

1,035 Views
mikedoidge
NXP Employee
NXP Employee

Hello @hicensezhang.

What is the version of the S32K144 SDK you are using? S32 SDK RTM 4.0.3 is the latest.

I see that the make command in your screen capture shows as: make -j4 all

However, when I build this same project, the make command is: make -j20 all

Did you change some settings on this project?

Best Regards,

Mike

0 Kudos
Reply