an internal error has occurred while add some dirver to the new project using S32DS3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

an internal error has occurred while add some dirver to the new project using S32DS3.4

2,058 Views
steven_zhang
Contributor V

I creat a new S32K344 procject in S32DS 3.4 IDE ,while adding some driver to the project with peripheral configure tool such as flexio_pwm,there in an internal error occured as blow:

内部错误.jpg

 the attatch is the log of the error.

0 Kudos
Reply
1 Reply

2,046 Views
mikedoidge
NXP Employee
NXP Employee

This post is a duplicate of https://community.nxp.com/t5/S32-Design-Studio/An-internal-error-has-occurred/m-p/1417596#M8238. All replies on this issue will be posted there.

0 Kudos
Reply