Why it is not possible to choose the package of the S32K144?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why it is not possible to choose the package of the S32K144?

1,456件の閲覧回数
javiervicandi
Contributor II

Why it is not possible to choose the package of the S32K144 when creating the project? Later we can add other CPU with the the right package (64 pins).

The clock manager component  does not show the clock values with 64 pins. If I switch (enabling) to the 100 pins and back to 64, I can see the values.

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,325件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Javier,

This is a limitation of S32 Design Studio Project Wizard. 

I've logged it as a new feature request into our tracking database.

Regarding clock manager:

This issue is addressed in the soon to be announced S32 SDK 0.9.0 release.

Regards

Stan

0 件の賞賛
返信