Why it is not possible to choose the package of the S32K144?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why it is not possible to choose the package of the S32K144?

1,768 次查看
javiervicandi
Contributor II

Why it is not possible to choose the package of the S32K144 when creating the project? Later we can add other CPU with the the right package (64 pins).

The clock manager component  does not show the clock values with 64 pins. If I switch (enabling) to the 100 pins and back to 64, I can see the values.

Thanks

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,637 次查看
stanish
NXP Employee
NXP Employee

Hi Javier,

This is a limitation of S32 Design Studio Project Wizard. 

I've logged it as a new feature request into our tracking database.

Regarding clock manager:

This issue is addressed in the soon to be announced S32 SDK 0.9.0 release.

Regards

Stan

0 项奖励
回复