Why it is not possible to choose the package of the S32K144?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why it is not possible to choose the package of the S32K144?

1,445 Views
javiervicandi
Contributor II

Why it is not possible to choose the package of the S32K144 when creating the project? Later we can add other CPU with the the right package (64 pins).

The clock manager component  does not show the clock values with 64 pins. If I switch (enabling) to the 100 pins and back to 64, I can see the values.

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,314 Views
stanish
NXP Employee
NXP Employee

Hi Javier,

This is a limitation of S32 Design Studio Project Wizard. 

I've logged it as a new feature request into our tracking database.

Regarding clock manager:

This issue is addressed in the soon to be announced S32 SDK 0.9.0 release.

Regards

Stan

0 Kudos
Reply