Who can send me the examples of the MPC5643L S32 project ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Who can send me the examples of the MPC5643L S32 project ?

1,807 次查看
edenli
Contributor V

Hi Guys,

 Nowdays,i am using the MPC5643L,but i can not find the C-code example about the MPC5643L for S32 project ,who can send me ?

标记 (3)
0 项奖励
回复
2 回复数

1,617 次查看
stanish
NXP Employee
NXP Employee

FYI:

There are some examples available here:

https://community.nxp.com/docs/DOC-329623 

There is no example for s32ds but it's easy to migrate it.

I'd suggest you to create a new empty project for MPC5643L in S32DS and transfer the source files + settings into the new project.

Hope it helps.

Stan

0 项奖励
回复

1,617 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can find one example in S32DS for PPC: File -> New -> New S32DS Project from Example -> Mixed_VLE_BookE_MPC5643L 

pastedImage_1.png

There is also example for motor control library here .

Jiri

0 项奖励
回复